For example, insert a rectangle on the SCR_UserScreen_1_1 page.
Click .

For example, insert a rectangle on the SCR_UserScreen_1_1 page. Click . ![]() |
Click in the properties access rights. Click . ![]() |
Assign the access rights as shown and confirm with OK. Click . ![]() |
You have assigned access rights to an object! |